I'd like to connect a USB endoscope or similar USB camera to the OM13098UL board with a LPC52628 chip, Is there an SDK example to test it? I don't need higth frame rate, but I need to extrat image info at least 2 times x second for proccess it. Thanks in advance
Hi,
You can try with the usb_device_video_virtual_camera example. The USB video virtual camera application is a simple demonstration program based on the MCUXpresso SDK. It is enumerated as a camera and users can see the video of the device by using a PC test tool.
This example can help as reference.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------