Maximum crystal series resistance of LPC4300

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Maximum crystal series resistance of LPC4300

1,180 次查看
yoshiyukiokada
Contributor III

I found something doesn't feel right with table data in LPC4300 datasheet.

In the table 41, "Recommended values for CX1/X2 in oscillation mode", there are two figures and they are same value " < 160ohm" on the line where Fundamental osccillation freq is 12MHz.

What is the difference between these two?

pastedImage_1.png

标签 (1)
0 项奖励
回复
1 回复

1,104 次查看
soledad
NXP Employee
NXP Employee

Hi, 

Yes, I think it is a mistake, but at the end, you know that we need to keep the Cext and Z of the Oscillator in the same value in order to get the resonance of the crystal oscillator.

Regards

Soledad

0 项奖励
回复