Maximum crystal series resistance of LPC4300

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum crystal series resistance of LPC4300

565 Views
yoshiyukiokada
Contributor III

I found something doesn't feel right with table data in LPC4300 datasheet.

In the table 41, "Recommended values for CX1/X2 in oscillation mode", there are two figures and they are same value " < 160ohm" on the line where Fundamental osccillation freq is 12MHz.

What is the difference between these two?

pastedImage_1.png

Labels (1)
0 Kudos
1 Reply

489 Views
soledad
NXP Employee
NXP Employee

Hi, 

Yes, I think it is a mistake, but at the end, you know that we need to keep the Cext and Z of the Oscillator in the same value in order to get the resonance of the crystal oscillator.

Regards

Soledad

0 Kudos