Hi to you all, 
I'm trying to use the LPC4370 (lpc link2 evaluation) in dual core mode: M4+M0App.
I have errors which I can not understand while compiling the M4 (master) project.
Here's the output for the memory map after compiling the m0app project:
Building target: mc_tut_m0app.axf
Invoking: MCU Linker
arm-none-eabi-gcc -nostdlib -[...]
Memory region Used Size Region Size %age Used
SPIFI2: 2224 B 512 KB 0.42%
RamLoc72: 16 B 72 KB 0.02%
This is as I expected.
But after M4 compiles:
Building target: mc_tut_m4xm0app1.axf
Invoking: MCU Linker
arm-none-eabi-gcc -nostdlib -[...]
Memory region Used Size Region Size %age Used
RamLoc128: 16 B 128 KB 0.01%
RamAHB32: 0 GB 32 KB 0.00%
RamAHB16: 0 GB 16 KB 0.00%
RamAHB_ETB16: 0 GB 16 KB 0.00%
RamM0Sub16: 0 GB 16 KB 0.00%
RamM0Sub2: 0 GB 2 KB 0.00%
RamLoc72: 0 GB 72 KB 0.00%
SPIFI1: 5516 B 512 KB 1.05%
SPIFI2: 2224 B 512 KB 0.42%
The RamLoc72 is not used and I got the following error.
c:/nxp/lpcxpresso_8.2.2_650/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: M0APP execute address differs from address provided in source image
collect2.exe: error: ld returned 1 exit status
make: *** [mc_tut_m4xm0app1.axf] Error 1
As I put in bold, the Master project is correctly allocating the Slave M0App code in the 2nd (external) Flash, as I asked during the creation wizard.
What is going on here? 
I attach here the docs I'm using.
Best,
Andrea
Hello Andrea,
In M4 project, please put RamLoc72 part at second RAM ( follow RamLoc128) to have a try.
If still have this error, please send your project to me, I will help you to check it on my side.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
 Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Alice,
I tried buy I got the same error. I attach my project files to the main question.
Hello Andrea,
I have help you change the memory setting of M4 project. The memory M0 project used, we need
put them into second flash part and second RAM part:
Please test the project I attached, hope it helps.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
 Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------