MMA8652FC or ILI9341 library example/demo projects?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMA8652FC or ILI9341 library example/demo projects?

1,295 Views
chrisdunn
Contributor I

Are there any example/demo projects that use the MMA8652FC or ILI9341 libraries that are part of the LPC55S69 SDK package?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,246 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Chris,

Because there is MMA8652 accelerator sensor on the LPC55S69-EVK, so there is driver and example code based IIC driver for LPC55S69 in SDK package as the following Fig:

pastedImage_1.png

But because LPC family has on-chip LCD controller for some processor, so we do not have ILI9341 chip on LPC board, so I suppose that we do not have driver of ILI9341 chip in SDK package.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply