MCUXpresso IDE JLink Debugger launch config

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCUXpresso IDE JLink Debugger launch config

跳至解决方案
671 次查看
robberpen
Contributor III

Hi

I study debug tool on MCUXpresso IDE User Guide. and interesting about Debug seting "SEGGER Jlink" below. But I have no idea how to lanuch Dailog from instruction below.

What is "lauch config file"?

image.png

0 项奖励
回复
1 解答
630 次查看
Alex_Wang
NXP Employee
NXP Employee

Hi, @robberpen 

The "launch config file" is a configuration file that is used to set and configure the parameters of a debugger such as SEGGER Jlink at startup. This file usually contains information about the target device to which the debugger is connected, debugging interface Settings, and so on.

Alex_Wang_0-1712887351726.jpeg

Best regards, Alex

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
631 次查看
Alex_Wang
NXP Employee
NXP Employee

Hi, @robberpen 

The "launch config file" is a configuration file that is used to set and configure the parameters of a debugger such as SEGGER Jlink at startup. This file usually contains information about the target device to which the debugger is connected, debugging interface Settings, and so on.

Alex_Wang_0-1712887351726.jpeg

Best regards, Alex

 

0 项奖励
回复