MCU-Link SWO ITM Console not flushing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCU-Link SWO ITM Console not flushing

1,068件の閲覧回数
briandavidson1
Contributor II

Hi!

After some fiddling with the debug settings the MCU-Link finally works. Poor OOB-experience, btw...

However, the SWO-ITM log doesn't behave as expected. When stepping through this example code:

 

    PRINTF("Hello World\r\n");

    /* Force the counter to be placed into memory. */
    volatile static int i = 0 ;
    /* Enter an infinite loop, just incrementing a counter. */
    while(1) {
        i++ ;
        PRINTF("i: %d\r\n", i);
        /* 'Dummy' NOP to allow source level single stepping of
            tight while() loop */
        __asm volatile ("nop");
    }

 

the first time SWO log shows up is at iteration 51:

 

Hello World
i: 1
i: 2
[...]
i: 50
i: 51

 

 

On the PE-Multilink the SWO ITM Console is updated on every line, which is expected, as there is a "\r\n" in every print command and this should flush the output.

Is there any way to make MCU-Link behave correctly?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,042件の閲覧回数
briandavidson1
Contributor II

No, the MCU keeps running fine. The SWO output is buffered in MCU-Link until approximately iteration 51 and only then the whole Console output is shown all at once.

With the PE Multilink the output of the ITM Console is updated on every iteration and each line shows up immediately.

To rephrase this: If I add a delay of 1s in betweeen, then it would take roughly one minute for the MCU-Link to show the output and all ~50 lines show up at the same time.

With the PE Multilink I'll see one line showing up each second, which is the desired bahaviour.

0 件の賞賛
返信

1,029件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I see your issue. Maybe it is a bug of firmware of MCU-Link device.

BR

XiangJun Rong

0 件の賞賛
返信

1,052件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Do you mean that the MCU stops at the i:51? If it is the case, can you try to declare the i as a global variable?

int i;

void main(void)

{

i=0;

while(1) {
        i++ ;
        PRINTF("i: %d\r\n", i);
        /* 'Dummy' NOP to allow source level single stepping of
            tight while() loop */
        __asm volatile ("nop");
    }

Pls have a try.

BR

XiangJun Rong

 

0 件の賞賛
返信