M4 & M0 cores communication via SDRAM or IPC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

M4 & M0 cores communication via SDRAM or IPC

470 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by maszup on Sat Apr 13 15:07:18 MST 2013

I'm begginer using LPC4357 with lpcxpresso and dual core. i have made both axf files and upladed them to both cores flash.


I'm trying to synchronize both cores in my software.


First i decided to try using SDRAM. M4 is reading first 4bytes of SDRAM and M0 is writing to that bytes but M4 goes immediately to Hard Fault. I don't know if it is possible to read & write SDRAM with two cores in the same time?


//M4


uint32_t *temp = (uint32_t*)SDRAM_BASE;


while(1) {


sprintf(buff, "value = %d\r\n", temp[0]);


console_sendString(buff);


TIM_Waitms(1000);


}


 


//M0


uint32_t *temp = (uint32_t*)SDRAM_BASE; 


uint32_t idx =0; 


 while(1) {


  temp[0] = idx++%100000; 



but on cosole i get some rubbish like "<0><0><0><0><0><0><0><0><0><0><0><0><0><0><0><0>" and console stops, probably M4 goes to hard fault . WHat is going on here?


 


Then i thought of using IPC but i do not have examples under LPCxpresso only under Keil. The example of IPC is nice but it is using M0 image read from CM0_image.c file  and M4 is uploading this image to M0. I do not know how to generate such a file in LPCxpresso. The examples is here:


<a href="http://www.lpcware.com/content/nxpfile/an11177-inter-processor-communication-lpc43xx">http://www.lpcware.com/content/nxpfile/an11177-inter-processor-communication-lpc43xx </a>

标签 (1)
0 项奖励
回复
0 回复数