Lifecycle of LPC2387FBD100 and LPC2478FBD208

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lifecycle of LPC2387FBD100 and LPC2478FBD208

1,738件の閲覧回数
friedrichermert
Contributor I

Hello,

can someone give me more information to the product LifeCycle (PLC) of these two LPC's?

LPC2478FBD208,551

and

LPC2387FBD100,551

Can i be sure, that i am able to buy these controllers for maybe the next 10 years?

I can only find the Notation "ACTIVE" für the LPC's.

Best regards,

Friedrich Ermert

ラベル(3)
2 返答(返信)

1,448件の閲覧回数
converse
Senior Contributor V

Try the product longevity table

Product Longevity: NXP LPC microcontrollers|NXP 

Looks like it is 2023/4 for your parts...

1,448件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Friedrich,

The link provided by Con Verse, it is correct the annoucement about the change in the longevity program for the LPC just happen at the beginning of 2017.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信