Latest non-demo version of BmpCvt.exe

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Latest non-demo version of BmpCvt.exe

2,036件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giusloq on Mon Apr 27 06:46:15 MST 2015
The tool BmpCvt tool inside emWin package from NXP is v5.14.

The current release is v5.28 (downloadable as demo version from emWin website).

Now I'd like to use the latest version, but demo version shows a splash screen that must be closed by pushing on Ok button. This is tedious when using a batch script that automatically converts 10-20 images.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,738件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giusloq on Tue Apr 28 02:15:56 MST 2015
It is certainly a newer version than the one I was using. But it isn't the latest.

Why doesn't NXP think to release emWin tools as a separate package? In this way, it's simpler to keep them updated, without changing BSPs.
0 件の賞賛
返信

1,738件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Apr 27 08:54:44 MST 2015
Hi giusloq,
Below BSP link contains 5.22 version of the tool. May be you want to use this version.
http://www.lpcware.com/content/nxpfile/emwin-522-board-support-package-ea1788-board
0 件の賞賛
返信