Latest non-demo version of BmpCvt.exe

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Latest non-demo version of BmpCvt.exe

2,083 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giusloq on Mon Apr 27 06:46:15 MST 2015
The tool BmpCvt tool inside emWin package from NXP is v5.14.

The current release is v5.28 (downloadable as demo version from emWin website).

Now I'd like to use the latest version, but demo version shows a splash screen that must be closed by pushing on Ok button. This is tedious when using a batch script that automatically converts 10-20 images.
标签 (1)
0 项奖励
回复
2 回复数

1,785 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giusloq on Tue Apr 28 02:15:56 MST 2015
It is certainly a newer version than the one I was using. But it isn't the latest.

Why doesn't NXP think to release emWin tools as a separate package? In this way, it's simpler to keep them updated, without changing BSPs.
0 项奖励
回复

1,785 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Apr 27 08:54:44 MST 2015
Hi giusloq,
Below BSP link contains 5.22 version of the tool. May be you want to use this version.
http://www.lpcware.com/content/nxpfile/emwin-522-board-support-package-ea1788-board
0 项奖励
回复