LPCXpresso54608 emWin support 10 inch LCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso54608 emWin support 10 inch LCD

524件の閲覧回数
gary12kuo
Contributor I

LPCXpresso54608 emWin is equipped with 4.3" LCD. If the LCD is changed to 8"~10" LCD,

then the emWin library can still support such a LCD without version updated/?

0 件の賞賛
返信
1 返信

474件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Gary,

emWin is Segger product, and it is supported by Segger. Please contact Segger for it.

emWin - The Embedded GUI by SEGGER | It simply works! 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信