LPCXpresso54018 OM40003 work with larger screens?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso54018 OM40003 work with larger screens?

1,108 次查看
RodrigoEngComp
Contributor I

Hey reader,

 

LPCXpresso54018 OM40003 work with larger screens?

 

I need a bigger screen, of the same type, with touch, does this board support such an application? And would NXP have this screen for sale?

 

Regards,

 

Rodrigo Almeida.

标签 (1)
0 项奖励
回复
1 回复

1,097 次查看
nxf77486
NXP TechSupport
NXP TechSupport

Hello @RodrigoEngComp ,

 The  LPCXpresso54018 support both Super-Twisted Nematic (STN) and Thin-Film Transistor (TFT) displays. Its has a dedicated DMA controller, and a programmable display resolution including 320 X 200, 320 X 240,

640 X 200, 640 X 240, 640 X 480, 800 X 600 up to 1024 x 768 pixels, and supports up to 24-bit true-color mode.

 

The larger size of LCD Panel supported for this LPC is 1024 x 768, the product that we currently have available compatible with your LPC product is in the link above and has the requirements that you need, but for a larger device you can purchase any other brand taking on account the dimensions and that it has to be either  Super-Twisted Nematic or Thin-Film Transistor.

 

RK043FN02H-CT: 4.3" LCD Panel

https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/4-3-lcd-panel:R...

0 项奖励
回复