LPCOpen for LPC1769 and MCUXpresso or LPCExpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPCOpen for LPC1769 and MCUXpresso or LPCExpresso

跳至解决方案
1,487 次查看
paulisammalisto
Contributor II

I have LPCXpresso board for LPC1769 and now I need SDK but I cannot find one for MCUXpresso and the link for LPCExpresso v2.07 does not work, "The system is currently unavailable."

0 项奖励
回复
1 解答
1,450 次查看
paulisammalisto
Contributor II

OK, I got it  to work, also the link worked today.

Thank you.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,217 次查看
kk7xo
Contributor III

How do I use LPCOpen for the LPC1769 with MCUXpresso for Visual Studio Code?

 

0 项奖励
回复
1,197 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello, the thread of this post has been closed. Please create a new case so that we can provide better support. 

0 项奖励
回复
1,463 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @paulisammalisto ,

Thanks for your post.

The demo code for LPC1769 is integrated in LPCOpen. Please refer to the following webpage:  LPCOpen Libraries and Examples | NXP Semiconductors 

About how to use LPCOpen with  MCUXpresso, you can also refer to the following content: MCUXpresso IDE - Using LPCOpen Examples | NXP Semiconductors 

LPCOpen is already integrated in the MCUXpresso IDE. There is no need for additional downloads. All you need to do is:
1. Open MCUXpresso IDE, then open the project as shown in the figure below:

 
Celeste_Liu_5-1739930953713.png
2. Select "lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769.zip". and then click "open".
 
Celeste_Liu_6-1739931069742.png
3. After the following interface appears, click "next".
 
Celeste_Liu_7-1739931121159.png
4.Finally, when the following interface appears, it's what you need.
 
Celeste_Liu_8-1739931174272.png
We hope the above information is useful to you.
 
BRs,
Celeste
 
---------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
---------------------------------------------------------------------------------------------------------------------
0 项奖励
回复
1,474 次查看
Dezheng_Tang
NXP Employee
NXP Employee
0 项奖励
回复
1,451 次查看
paulisammalisto
Contributor II

OK, I got it  to work, also the link worked today.

Thank you.

0 项奖励
回复