LPC845 FRO control register

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC845 FRO control register

1,870 次查看
lajostoth
Contributor II

Hi,

This is a snippet of 845 SDK :

845sdk.PNG

I can't find any information about [1:0] bits of FROOSCCTRL register in the user manual.

These data are confidential ?

845fro.PNG

0 项奖励
回复
4 回复数

1,512 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Lajos Toth,

These bits are set in the set_fro_frequency() API, this function is located in the boot ROM. In the SDK you can found it with the following name and the argument helps you to modify the output frecuency:

 CLOCK_SetFroOscFreq(kCLOCK_FroOscOut18M);   /*!< Set up FRO freq to 18MHz */

 CLOCK_SetFroOscFreq(kCLOCK_FroOscOut24M);   /*!< Set up FRO freq  to 24MHz*/

 CLOCK_SetFroOscFreq(kCLOCK_FroOscOut30M);   /*!< Set up FRO freq  to 30MHz*/

Hope it helps you,

Alexis Andalon

0 项奖励
回复

1,512 次查看
lajostoth
Contributor II

Thank you Alexis Andalon for your answer. The reason of my question was that I have trouble with get clock functions.

I created a simple USART project transmit data to VCOM port:code.PNG

This is clocks diagram of USART0:frg0.PNG

If I change CLOCK_GetFRG0ClkFreq() to 30000000U the usart works well, but the function returns  wrong value(13222784)

0 项奖励
回复

1,512 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Lajos Toth,

I think you're confusing the FRG Clock with the FRO clock, these are two diferent clock options.

In the USART_Init, you're using CLOCK_GetFRG0ClkFreq() but the original question is about the CLOCK_GetFroFreq()

Best Regard,

Alexis Andalon

0 项奖励
回复

1,512 次查看
lajostoth
Contributor II

Hi Alexis Andalon,

I am not confusing with clocks,  CLOCK_GetFRG0ClkFreq() call CLOCK_GetFroFreq() function if the clock source for FRG is setting to FRO. The problem is solved, there is a type casting bug in CLOCK_GetFRG0ClkFreq() function as well as in FRG1.

Best Regards

0 项奖励
回复