LPC824 - IRC - quoted 12MHz +/- 1.5%

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC824 - IRC - quoted 12MHz +/- 1.5%

784 Views
sanders7284
Contributor III

Is there any avalible graphed data showing typical curves?

Vs Voltage

Vs Temp

Vs ageing

Also is the following qualified? i.e. what is the accuracy below 2.7V?

"Conditions: Frequency values are typical values. 12 MHz  1.5 % accuracy is guaranteed for
2.7 V  VDD  3.6 V. Variations between parts may cause the IRC to fall outside the 12 MHz 
1.5 % accuracy specification for voltages below 2.7 V."

Labels (2)
0 Kudos
Reply
0 Replies