LPC824 - IRC - quoted 12MHz +/- 1.5%

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC824 - IRC - quoted 12MHz +/- 1.5%

754 次查看
sanders7284
Contributor III

Is there any avalible graphed data showing typical curves?

Vs Voltage

Vs Temp

Vs ageing

Also is the following qualified? i.e. what is the accuracy below 2.7V?

"Conditions: Frequency values are typical values. 12 MHz  1.5 % accuracy is guaranteed for
2.7 V  VDD  3.6 V. Variations between parts may cause the IRC to fall outside the 12 MHz 
1.5 % accuracy specification for voltages below 2.7 V."

标签 (2)
0 项奖励
回复
0 回复数