LPC812 XSON16 package information

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC812 XSON16 package information

1,454 次查看
jackhsu
Contributor III

Dear,

Good day.
I'm write the email that get more information about package XSON16.
We are IC programmer manufacturer, and we will support LPC812 with XSON16 for customer in China.
We are finding the socket on it. and the socket manufacturer ask us that he has to know the normal and minimum about the height of IC.
The height is only show maximum is 0.5mm, or let me know the tolerance about height of IC. Thanks.

There is the package information.
https://www.nxp.com/docs/en/package-information/SOT1341-1.pdf

标签 (1)
0 项奖励
回复
3 回复数

1,296 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Jack

This is 0.45 to 0.50 mm

Regards

Vicente

0 项奖励
回复

1,296 次查看
jackhsu
Contributor III

Hi Vicente,

Thanks for your reply.

Is the 0.45mm typical or minimum?

Thank you.

Regards,

Jack Hsu

0 项奖励
回复

1,296 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

0.45 mm is the minimum.

Regards

Vicente Gomez

0 项奖励
回复