LPC804 - Want to store some local information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC804 - Want to store some local information

ソリューションへジャンプ
1,162件の閲覧回数
biju_nair
Contributor III

Hi,

We would like to use the LPC804 to store some configuration information inside the controller. We will be running a small code in the controller and would like to store some configuration information also inside the controller. I see reference to AN12125_LPC802.zip in the community, where it can be used an an EEPROM, but there is no place from where i can download this, as the link seems to be broken. Can someone point me to a working link for this project ?

Regards, Biju

0 件の賞賛
返信
1 解決策
1,151件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @biju_nair,

You can look the AN12125 application note software at LPC80x NXP's website: LPC80x 15 MHz|Arm Cortex-M0+|32-bit Microcontrollers (MCUs) | NXP Semiconductors.

Please go to Documentation, check Application Note Software, and then search for the application note.

RaulRomero_1-1676573157360.png

Best regards, Raul.

元の投稿で解決策を見る

2 返答(返信)
1,138件の閲覧回数
biju_nair
Contributor III

Thanks much Raul. Appreciate your help.

Regards, Biju

0 件の賞賛
返信
1,152件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @biju_nair,

You can look the AN12125 application note software at LPC80x NXP's website: LPC80x 15 MHz|Arm Cortex-M0+|32-bit Microcontrollers (MCUs) | NXP Semiconductors.

Please go to Documentation, check Application Note Software, and then search for the application note.

RaulRomero_1-1676573157360.png

Best regards, Raul.