Hi,
I need to enter ISP mode with UART (flexcom 0)
Is it possible when a firmware is already in place on LPC55xx ?
After a reset, I send a "ping" command (5A A6), but I receive no response and the program in place launch.
The default CMPA is in "Auto ISP" mode
How to force CMPA to be in "UART ISP" mode without ISP pin ?
Note : When LPC55xx have no firmware, the "ping" command have a response ACK (5A A7 ...), because the LPC55xx goes into ISP mode automatically
Regards,
Phil