Hi
I have a couple questions regarding the PRINCE functionality of the LPC55Sxx series.
1. The manual says all the encrypted memory should be written at once. But that is not possible if I want to do a firmware upgrade, since the whole firmware would have to be placed into RAM first and then copied into flash, right? Can't I erase and write page by page when using encryption?
2. Reading the encrypted memory doesn't seem to work when using the ROM API. FLASH_Read() function returns garbage, whereas when I do a simple memcpy() I get the correctly decrypted data...
 
					
				
		
 Alice_Yang
		
			Alice_Yang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello @keepcoding
BR
Alice
Ok, but how do I write all data at once? The amount of data I want to write is larger than the available SRAM on the chip, so where should I put the data before "writing it to flash at once"?
 
					
				
		
 Alice_Yang
		
			Alice_Yang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello @keepcoding
Thanks for your reply.
I also checked our SDK demo, yes this is the limitation.
Check that the whole encrypted subregions will be writen at once. If not , will return Error.
BR
Alice
I did a quick test by using the normal erase and write functions to fill the encrypted region (write data chunk by chunk). This appears to be working just fine.
So now I'm wondering, why does the documentation state that it needs to be written at once? Is there something I don't see? Could you please shed some more light on this?
 
					
				
		
 Alice_Yang
		
			Alice_Yang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello @keepcoding
Please have a look at the below thread:
"According to UM11126(49.16.1 Functional details), each crypto region has its own SKEY and IV code. SKEY and IV are used together by the PRINCE when encrypting or decrypting the data in the sub-regions of crypto region.
For Instance, For PRINCE region1, each time after we execute erasing operation, new Skey1 and IV1 are generated, thus when executing erase/read/write operation to another sub-region, the old IV1 and new IV1 don’t match, which causes PRINCE can’t decrypt correctly."
BR
Alice