LPC55SXX secure boot and flash modification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC55SXX secure boot and flash modification

跳至解决方案
898 次查看
johannes_ferch
Contributor II

Hi everyone,

we have an application utilizing a LPC55S06 microcontroller into which we want to add secure boot and memory encryption functionality. 

Besides the regular firmware and some static datasets determined during compilation, we have some runtime data that we need to persist in on-chip flash. We were wondering if these use-cases are compatible with each other or if any write to flash would inevitably lead to a signature invalidation during the next secure boot cycle.

In other words, is it possible to let's say generate a binary containing all the static storage in flash pages 1 to x and configure PRINCE/secure boot to validate these memory sections but ignore another section x to y that are excempt from the initial .sb file for dynamic memory uses? 

Could you give some hints on how to setup the memory layout and configure the flash regions/encryption with the Secure Provisioning Tool?

Thanks in advance,
Johannes

0 项奖励
回复
1 解答
795 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi @johannes_ferch 

Thanks for your reply.

For the latest question, I have helped you create a new private ticket.

I will reply you on the new one.

Thank you.

 

BR

Alice

在原帖中查看解决方案

0 项奖励
回复
5 回复数
847 次查看
johannes_ferch
Contributor II

Hi Alice,

thanks for your reply and the provided resources.

I understood that there are different PRINCE regions for LPC55 family devices from the documentation, however it's not yet clear to me how PRINCE and secure boot work together. I've seen the corresponding drop-down menu in the Secure Provisioning Tool (see below), but can't come up with a mental model on my own. Which data is used during image validation during secure boot, just the regions that are initially programmed or the entire on-chip memory?

johannes_ferch_0-1754310253332.png

And maybe more specific to my current problem:

  1. Once secure boot is enabled, would any modification to the underlying memory invalidate secure boot signatures automatically due to hashes no longer matching? 
  2. Could this be circumvented by having spacial separation within the memory? For instance, having static content in one PRINCE region (e.g. 0 below) and dynamic data in another (e.g. 1 below)? 

johannes_ferch_1-1754311425568.png

 

 

 

 

 

 

For additional context/motivation, we would like to store a device-specific serial number onto every device within the dynamic data region which is not yet known during firmware/image creation. We want to still have the benefits of secure boot but don't want to loose the possibility to store some bytes of data. Or are these use cases not compatible and would we have to rely on some external memory IC here?

Thanks,
Johannes

 

0 项奖励
回复
828 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @johannes_ferch 

1) Once secure boot is enabled, would any modification to the underlying memory invalidate secure boot signatures automatically due to hashes no longer matching? 

->>During secure boot, the entire flash is not validated. You can specify the length of the secure image.

2) Could this be circumvented by having spacial separation within the memory? For instance, having static content in one PRINCE region (e.g. 0 below) and dynamic data in another (e.g. 1 below)? 

 ->> YES.

3) Regarding your usage, I recommend that you describe your requirements and application details, and we will provide you with suggestions.

 

Thank you.

 

BR

Alice

808 次查看
johannes_ferch
Contributor II

Hi @Alice_Yang,

thanks for your reply, this information is already really helpful!

Appreciate your assistance on providing suggestions based on our use-case/requirements. I've tried to roughly visualize and describe what we're trying to achieve in the following overview and a memory layout (we can of course adjust if that makes things easier technically):

johannes_ferch_0-1754567390286.png

Item 1 contains our business logic that gets built from the source code into a regular binary file. After compliation and linking, we take the resulting hexfile and append some static data (Item 2: characteristic maps, lookup tables, etc. that we need for our application) in a post-build step which results in a combined .hex-file of code and static information. This is the artifact that we want to have a secure boot image over, that gets signed and verified during device startup. 

In Item/Region 3 we want to be able to store a bit of dynamic data that is device specific and cannot be part of the device-generic artifact above. Our production workflow would program the artifact above onto every unit and subsequently execute the application. Once running, we use a serial protocol to provide unit specific information like a serial number, lot number, etc. that is retrieved during production over UART and persist them in non-volatile memory. This information is not modified afterwards. In the end, units are then packaged and shipped. 

Once deployed in the field, we would also like to persist some usage time information into the same dynamic region during runtime (just some usage time tracking etc. in a ring buffer, nothing special). We take different memory sections to not interfere with the information provided during production. 

1. Do you have any specific recommendations we should take into account for this?

2. Would something like this make sense for the PRINCE configuration?

johannes_ferch_0-1754576395657.png

3. I've looked at the SDK example for PRINCE en-/decryption you referred to - in which circumstances do we need to include functions like 'PRINCE_FlashProgramWithChecker'? Could we also leave region 2 in the configuration disabled if we don't need encryption and avoid this additional complexity?

Thanks a lot in advance,
Johannes

0 项奖励
回复
796 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi @johannes_ferch 

Thanks for your reply.

For the latest question, I have helped you create a new private ticket.

I will reply you on the new one.

Thank you.

 

BR

Alice

0 项奖励
回复
877 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @johannes_ferch 


Yes, PRINCE can be configured to encrypt different memory regions.

Alice_Yang_0-1754042549498.png

A PRINCE demo is available in the SDK—please refer to it for implementation details.

Detail please refer to:  UM -> "44.17 PRINCE real-time encryption or decryption details".


For  secure boot using the SEC tool, you can refer to the thread below.

https://community.nxp.com/t5/MCX-Microcontrollers-Knowledge/MCUXN947-Security-Configuration-Secure-B...  

 Thank you.

 

BR

Alice

0 项奖励
回复