LPC55S6x High-speed PHY

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S6x High-speed PHY

996 次查看
dingelen
Contributor III

Hi,

in the datasheet, for activating the high-speed PHY, it is mentioned the the 32k_osc should be activated. In the clock description section it is mentioned that this can be the FR32K or the XTAL32K.

Does it matter which of both is used for the High-speed PHY? I prefer not to add an extra external 32kHZ oscillator.

Thanks!

Tom

标签 (2)
0 项奖励
回复
1 回复

909 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Tom,

 

You could use either external XTAL32K or internal FRO32K selecting from RTCOSC32KSEL register.

pastedImage_2.png

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复