LPC55S69 : temperature settling time

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69 : temperature settling time

826 次查看
EugeneHiihtaja
Senior Contributor I

Hello !

in DS is specified settling time of temperature sensor after power on in table 12.2.2

but what about settling time after Power-Down mode and actual conversion time ?

How fast after resuming from  Power-down mode I can get good measurement of temperature ?

Regards,

Eugene

0 项奖励
回复
1 回复

779 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Eugene,

As you may notice, this measure is not characterized but I think it would be a good aproximation to use the same setting time as the one from power-up. Also, this is an analog sensor connected to the channel 26 in the ADC so check the chapter 39.7.6 in the reference manual for more information about it.

Best Regards,

Alexis Andalon

0 项奖励
回复