Hi
I'm trying to store the PUF activation code/userKeyCode in the KeyStore
To that order i've filled the ffr_key_store_t 3 pages as
uint32_t magic;
uint32_t pufDischarge;
uint8_t activationCode[1192];
uint8_t SBKEK[56];
uint8_t USERKEK[56];
uint8_t reserved[56];
uint8_t prince0[56];
uint8_t prince1[56];
uint8_t prince2[56];
filled with all zeroes except activationCode, UserKEK and magic set to 0x95959595
and then called FFR_KeystoreWrite
After reboot, the unit does not respond any longer to SWD or even ISP/USB-HID
It behaves as if CMPA settings where filled with incorrect value, while i only modified the KeyStore part
(i did not touch the other CMPA main parts)
I was under the impression that it was ok to set activation code and user Keycode and set magic to 0x9595.... as many time as i want until CMPA is locked
Isn't that correct ?
What is the right way to set activation code & friends ? Set all CMPA field + keyStore at the same time ?
Thank you in advance
Tres
Hello again
So i did try with the bldhost examples given in the applicaiton note => worked fine and only changed the keystore as expected
Using Bldhost => works as expected
Just calling FFR_KeystoreWrite() to store the keyStore with created entries => bricked MCU. So either i misused it/misunderstood it or the call is having side effects.
Google was of little help, FFR_KeystoreWrite does not seem to be used much.
Is there any demo/sample code known to work available for FFR_KeystoreWrite() ?
Thank you in advance
Tres
Hello,
The right PFR key store layout is shown below:
Address |
Size (bytes) |
Name |
Description |
0x9E600 |
4 |
Key Store Header |
Marker. A value of 0x95959595 means that Activation code is valid. |
0x9E604 |
4 |
PUF Discharge time |
Time in milliseconds to wait until PUF SRAM fully discharges. Only effective when PUF Start fails. Set to zero to use default discharge time. |
0x9E608 |
1192 |
Activation Code |
Device specific PUF activation code generated by enroll command during key provisioning. |
0x9EAB0 |
4 |
SBKEK Key Code Header |
Marker. A value of 0x59595959 means that key code is valid. |
0x9EAB4 |
52 |
SBKEK Key Code |
Key Code for wrapped SBKEK key |
0x9EAE8 |
4 |
USERKEK Key Code Header |
Marker. A value of 0x59595959 means that key code is valid. |
0x9EAEC |
52 |
USERKEK Key Code |
Key Code for wrapped USERKEK key |
0x9EB20 |
56 |
- |
Reserved. |
0x9EB58 |
4 |
PRINCE Region 0 Key Code Header |
Marker. A value of 0x59595959 means that key code is valid. |
0x9EB5C |
52 |
PRINCE Region 0 Key Code |
Key Code for wrapped PRINCE Region 0 key |
0x9EB90 |
4 |
PRINCE Region 1 Key Code Header |
Marker. A value of 0x59595959 means that key code is valid. |
0x9EB94 |
52 |
PRINCE Region 1 Key Code |
Key Code for wrapped PRINCE Region 1 key |
0x9EBC8 |
4 |
PRINCE Region 2 Key Code Header |
Marker. A value of 0x59595959 means that key code is valid. |
0x9EBCC |
52 |
PRINCE Region 2 Key Code |
Key Code for wrapped PRINCE Region 2 key |
Other KC fileds which are not used can be filled 0.
BR
Alice
Hello trescurieux,
It seems there is something wrong in the User Manual, doesn't give the KC header,
I will confirm it with internal.
And I sorry i'm mistake, the function "ffr_get_customer_data" can't read keystore data,
need use "ffr_keystore_get_kc", but I recommend you use blhost to write KC/AC, because the ffr_keystore_write need program 3 pages, must configure all the 3 pages well, Blhost can program one KC alone.
BR
Alice
Thank you, but
The thing is, i didnt modify CMPA directly
I only wrote KeyStore through one call to FFR_KeystoreWrite, that's it.
Does that trigger an implicit CMPA writing with random value(s) or zeroes ?
Is there a way to put stuff in the keyStore without altering the CMPA page for test purpose ?
Thank you
Hello trescurieux,
Sorry there isn't a demo.
There are some points you need pay attention:
1) "filled with all zeroes except activationCode" -> Fill zeroes are not right.
2) The second parameters of ffr_keystore_write need point 3 pages structure.
So, I suggest you using ffr_get_customer_data() first read the 3 pages that includes AC/KC from your chip, then just change the AC /KC part, then use ffr_keystore_write() write the three pages.
BR
Alice
Hi
Thank you for the pointer , so i tried calling :
FFR_GetCustomerData(&_config,tmp+0*512,1*512,512 );
to get the page after cmpa (i.e. first page of keystore)
It failed with error 4 (invalid arg i think). Both flash_init and FFR_Init have been called previously successfully.
Is there alignment constraint on the target buffer in ram ?
For reference, i just want to store AC and userKEK in PFR without activating prince or anything else.
Just write the 3 keystore pages, that's it.
Thank you in advance
Tres
Hello,
Yes, when write CMPA, you need very carefully, you can see the CMPA includes many parts in attached excel of UM, for example ISP mode, if disable ISP mode by mistake, it can't enter ISP mode.
It sees you use PUF with Prince, you can refer to this AN:
https://www.nxp.com.cn/docs/en/application-note/AN12527.pdf
BR
Alice