LPC55S69 ROM bootloader hangs if Flash operations are interrupted

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69 ROM bootloader hangs if Flash operations are interrupted

1,636 次查看
awseiger
Contributor I

I have an LPC55S69 set up to boot a recovery SB2.1 image from SPI Flash. This recovery image is loaded into SRAM and executes, copying a fallback image from another location in SPI Flash to 0x0 in the internal flash. 

If I power-cycle the processor while my recovery image code is copying the fallback image to internal flash, the ROM bootloader does not enter SPI Flash Recovery mode or ISP Mode - it simply hangs until I pull ISP low. As soon as I pull ISP low, it begins SPI Flash Recovery as I would have expected it to do immediately upon power-up.

How can I fix this? I am trying to use the SPI Flash Recovery feature as a way to prevent in-field bricking during a power loss, and requiring the ISP pin to be pulled low to un-brick a device is not acceptable for our application.

标签 (1)
0 项奖励
回复
4 回复数

1,594 次查看
awseiger
Contributor I

Through other channels, I have arrived at this being an issue as well. Are there any work-arounds or planned fixes from NXP?

0 项奖励
回复

1,580 次查看
FelipeGarcia
NXP Employee
NXP Employee

Unfortunately, we do not have information of any plans for fixing this issue in the future. I am sorry for the inconvenience this may cause you.

Best regards,

Felipe

0 项奖励
回复

1,573 次查看
bobpaddock
Senior Contributor III

"Unfortunately, we do not have information of any plans for fixing this issue in the future"

This is driving people like me away from designing in NXP parts.


Never taking time to fix known issues, and leaving people to stumble into the known issues after committing resources to a NXP part.  List the issues right in the datasheets as soon as they are found.

 

 

 

0 项奖励
回复

1,599 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

I noticed in our ticket system that you have discovered errata ROM.5 that indicates that this is caused if an image is corrupted or with flash pages in an erased or unprogrammed state, the ROM fails to enter ISP mode. This also makes sense to me as the power loss may be corrupting the image you are loading so you enter the errata scenario.

Best regards,

Felipe

0 项奖励
回复