LPC55S69 : FMC configuration register

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69 : FMC configuration register

1,136 次查看
EugeneHiihtaja
Senior Contributor I

Hello !

I can see in all examples in SDK is only FLASHTIM is set .

But what about enable flash prefetch and acceleration bits ?

They never enabled. Why ? They should work with silicon 1B.

How to handle those ?

Can I enable those at the same time when FLASHTIM is changed ?

Should I invalidate/flush those caches when use Flash API from Bootrom ?

Or when I encrypt/decrypt on fly if PRINCE peripheral is in use.

In K82 time it was always separate API to handle those issues.

Regards,

Eugene

0 项奖励
回复
2 回复数

1,046 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello Eugene, 

But what about enable flash prefetch and acceleration bits ?

They never enabled. Why ? They should work with silicon 1B.

Yes you should be able to enable these without a problem. The SDK examples are not designed to show the optimum behavior, instead we provide base examples that show how the peripherals should work. Though any additional modifications to optimize or customize should be made by customers.

How to handle those ?

Can I enable those at the same time when FLASHTIM is changed ?

You may enable them as you mention. However please consider the following points.

pastedImage_5.png

Please confirm the revision you are working with and disable the prefetch bit must be disabled prior to executing flash commands.

Best Regards,

Sabina

0 项奖励
回复

1,046 次查看
EugeneHiihtaja
Senior Contributor I

Hi Sabina !

Yes, I have A2 board revision and expect there 1B version of bootloader.

Regards,

Eugene

0 项奖励
回复