LPC55S69-EVK not flashing, Heating issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69-EVK not flashing, Heating issue

4,220 次查看
rkulkarni
Contributor I

When running the internal ADC, the input voltage went out of range for 2-3 seconds (around 20V). After that, I am unable to flash the board. I am getting the error below:

Unable to connect wire for probe index 1.
Error: Wire Ack Fault - target connected?


Unable to connect wire for probe index 1.
Error: Wire Ack Fault - target connected?

Error: Wire Ack Fault - target connected?

at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.checkServerReply(RedlinkServerClient.java:227)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.wireConnect(RedlinkServerClient.java:1281)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.jtag.AbstractJtagDiscovery.ideConnect(AbstractJtagDiscovery.java:240)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.jtag.AbstractJtagDiscovery.connect(AbstractJtagDiscovery.java:196)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.jtag.AbstractJtagDiscovery.discover(AbstractJtagDiscovery.java:155)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.TargetDiscovery.jtagDiscovery(TargetDiscovery.java:454)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.TargetDiscovery.configureEmulator(TargetDiscovery.java:155)
at com.nxp.mcuxpresso.core.debug.support.linkserver.flash.LinkServerFlashWorkItem.buildCommand(LinkServerFlashWorkItem.java:256)
at com.nxp.mcuxpresso.core.debug.launch.AbstractNXPLaunchConfigHandler.scheduleOperation(AbstractNXPLaunchConfigHandler.java:879)
at com.nxp.mcuxpresso.core.debug.launch.AbstractNXPLaunchConfigHandler.openFlashDialog(AbstractNXPLaunchConfigHandler.java:593)
at com.nxp.mcuxpresso.core.debug.ui.FlashToolMenuDelegate.execute(FlashToolMenuDelegate.java:146)
at org.eclipse.ui.internal.handlers.HandlerProxy.execute(HandlerProxy.java:283)
at org.eclipse.ui.internal.handlers.E4HandlerProxy.execute(E4HandlerProxy.java:97)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
at java.base/java.lang.reflect.Method.invoke(Unknown Source)
at org.eclipse.e4.core.internal.di.MethodRequestor.execute(MethodRequestor.java:58)
at org.eclipse.e4.core.internal.di.InjectorImpl.invokeUsingClass(InjectorImpl.java:317)
at org.eclipse.e4.core.internal.di.InjectorImpl.invoke(InjectorImpl.java:251)
at org.eclipse.e4.core.contexts.ContextInjectionFactory.invoke(ContextInjectionFactory.java:173)
at org.eclipse.e4.core.commands.internal.HandlerServiceHandler.execute(HandlerServiceHandler.java:156)
at org.eclipse.core.commands.Command.executeWithChecks(Command.java:488)
at org.eclipse.core.commands.ParameterizedCommand.executeWithChecks(ParameterizedCommand.java:485)
at org.eclipse.e4.core.commands.internal.HandlerServiceImpl.executeHandler(HandlerServiceImpl.java:213)
at org.eclipse.e4.ui.workbench.renderers.swt.HandledContributionItem.executeItem(HandledContributionItem.java:438)
at org.eclipse.e4.ui.workbench.renderers.swt.AbstractContributionItem.handleWidgetSelection(AbstractContributionItem.java:449)
at org.eclipse.e4.ui.workbench.renderers.swt.AbstractContributionItem.lambda$2(AbstractContributionItem.java:475)
at org.eclipse.swt.widgets.EventTable.sendEvent(EventTable.java:89)
at org.eclipse.swt.widgets.Display.sendEvent(Display.java:4251)
at org.eclipse.swt.widgets.Widget.sendEvent(Widget.java:1066)
at org.eclipse.swt.widgets.Display.runDeferredEvents(Display.java:4068)
at org.eclipse.swt.widgets.Display.readAndDispatch(Display.java:3645)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine$5.run(PartRenderingEngine.java:1155)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.e4.ui.internal.workbench.swt.PartRenderingEngine.run(PartRenderingEngine.java:1046)
at org.eclipse.e4.ui.internal.workbench.E4Workbench.createAndRunUI(E4Workbench.java:155)
at org.eclipse.ui.internal.Workbench.lambda$3(Workbench.java:644)
at org.eclipse.core.databinding.observable.Realm.runWithDefault(Realm.java:338)
at org.eclipse.ui.internal.Workbench.createAndRunWorkbench(Workbench.java:551)
at org.eclipse.ui.PlatformUI.createAndRunWorkbench(PlatformUI.java:156)
at org.eclipse.ui.internal.ide.application.IDEApplication.start(IDEApplication.java:152)
at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:136)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:402)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at java.base/jdk.internal.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
at java.base/jdk.internal.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
at java.base/java.lang.reflect.Method.invoke(Unknown Source)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:659)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:596)
at org.eclipse.equinox.launcher.Main.run(Main.java:1467)

Also, the board is heating near the USB ports when connected to debug port or the +5V power supply port. Does this mean that there is some component failure on board or is there some other issue?

标签 (1)
0 项奖励
回复
3 回复数

4,167 次查看
frank_m
Senior Contributor III

> Also, the board is heating near the USB ports when connected to debug port or the +5V power supply port.

I suspect the overvoltage has fused protective elements/diodes at the affected MCU GPIOs.
This usually creates a short circuit, pushing the power supply to the limits.

As said, perhaps you could get away with unsoldering the MCU, and replace it with a new one.

0 项奖励
回复

4,175 次查看
ErichStyger
Specialist I

As you applied 20V to the device, you have for sure destroyed the MCU, probably other parts of the EVK too.

You might be lucky and only the LPC55S69 MCU is damaged. In this case, you could unsolder the MCU and populate it with a new part.

You better get a board replacement.

0 项奖励
回复

4,181 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @rkulkarni 

The input voltage is too high to damage the chip.

It is better for input voltage is lower than 3.6V.

For your this board, you can try to enter ISP mode, use blhost, check whether can connect.

If failed, the chip is broken.

 

BR

Alice

 

0 项奖励
回复