LPC55S69 : BoD type of Reset reason

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69 : BoD type of Reset reason

1,106 次查看
EugeneHiihtaja
Senior Contributor I

Hello !

In UM chapter 4.6.1 is mentioned that Brown Out Detect (BOD) type of reset can be detected.

But it is not so clear if something should be enabled beforehand.

I have plan to keep MCU in Power-down mode and expect if voltage go to low ( but not 0) and return back, reset is happens and via reset reason will be clear that case.

It would be nice to have BoD as wakeup source from Power-Down mode of MCU but it is not possible.

But how to configure MCU for detect BoD type of reset.

Regards,

Eugene

0 项奖励
回复
1 回复

1,042 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello Eugene,

For topics that are similiar please keep the questions on one thread. If you have follow up questions you may reply in the same posts regarding the same information.

For the answer to this post please refer to the community post.

https://community.nxp.com/thread/517253 

Best Regards,

Sabina

0 项奖励
回复