LPC55S28 Schematic review request

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC55S28 Schematic review request

跳至解决方案
808 次查看
steve5528
Contributor I

Greetings!

I'm in the process of designing my first LPC55S28 board with fairly modest goals, as follows:

  1. Power the MCU with MCU-link pro debug probe
  2. Flash sample programs to MCU via debug probe
  3. Test blinking led, and button operations
  4. Test UART functionality thru VCOM facility of debug probe

Here is the schematic, and I would appreciate your review comments - it would be great to have the board working "right in the first pass" as NXP doc says.

nxp-review-lpc55s28-pcb-v1.jpg

 

I have two follow-up questions:

  1. Is ISP support needed for the board if flashing is done mainly with MCU-link pro?
  2. Is there a command line version of MCU-link pro to flash the device without having to invoke the IDE?

Thanks much in advance!

0 项奖励
回复
1 解答
790 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @steve5528,

1. Technically you would not need ISP support, but it is highly recommended to include it for anything that might go wrong while programming the MCU.

2. You could use LinkFlash, which is a GUI based on LinkServer to flash NXP devices, which is based on command line. If you have the latest version of MCUXpresso installed (v24.12.148), you should also have LinkFlash v24.12.21 installed already.

BR,
Edwin.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
791 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @steve5528,

1. Technically you would not need ISP support, but it is highly recommended to include it for anything that might go wrong while programming the MCU.

2. You could use LinkFlash, which is a GUI based on LinkServer to flash NXP devices, which is based on command line. If you have the latest version of MCUXpresso installed (v24.12.148), you should also have LinkFlash v24.12.21 installed already.

BR,
Edwin.

0 项奖励
回复
781 次查看
steve5528
Contributor I

Hello @EdwinHz 

Great. I will incorporate the ISP into schematics. Need to upgrade IDE so linkflash is installed.

 

Hopefully you or someone at NXP can comment on the schematics as well.

0 项奖励
回复
759 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @steve5528,

I apologize for missing the schematic review. It looks OK!

 

0 项奖励
回复
736 次查看
steve5528
Contributor I

Hi @EdwinHz  Thank you.

0 项奖励
回复