Hi,everyone:
It is solved,thanks!
I have another question,
Why is it causing such an error, can someone tell me?
thanks!
====================================
Hi, everyone :
How to solve the error generated under debug ????
Both types of programming using MCU-LIN PRO or EVK-LINK2 produce the same error, thanks!!
LINK2 Debug :
MCU-LINK PRO Debug :
How to solve the error, thanks !!!
I perform the same steps in another LPC55S16-EVK , it’s okay in another LPC55S16-EVK , No error occurred
已解决! 转到解答。
Hello emmt55s16,
Please erase the flash first, using GUI Flash tool
If still can't work, enter ISP mode using Flash Magic to erase.
Or try to hold on ISP pin when reset board, and do not release until finish debug.
BR
Alice
Hello emmt55s16,
Please erase the flash first, using GUI Flash tool
If still can't work, enter ISP mode using Flash Magic to erase.
Or try to hold on ISP pin when reset board, and do not release until finish debug.
BR
Alice
Hi @Alice_Yang , using mimxrt595 and have the same problem, also tried to erase the flash memory through GUI tool, it doesn't detecting the probe (using mcuexpresso IDE and Linux),
Even after entering into the ISP mode, probe is not detecting, Hence i'm not able to erase the flash memory.