LPC55S16-EVK Evaluation Board is not going in ISP mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S16-EVK Evaluation Board is not going in ISP mode

1,756 Views
VChaudhary
Contributor III

We purchased three LPC55S16-EVK Evaluation Boards, Two of them are not going in ISP mode. We tried to holding ISP
button down while pressing and releasing Reset (SW2) to force the
LPC55Sxx into ISP mode.

I also tried installing JS3 Jumper. But no luck. below is the response of blhost.

C:\Projects\XCOM\BT>blhost.exe -p COM3 get-property 1
Ping responded in 1 attempt(s)
Inject command 'get-property'
Error: read_start_byte() timeout after 5.178 seconds
sendCommandGetResponse.writePacket error 5.
Response status = 10004 (0x2714) No response packet from target device.

Thanks

0 Kudos
Reply
5 Replies

1,697 Views
VChaudhary
Contributor III

Mass erasing doesn't resolve the issue.

0 Kudos
Reply

1,670 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I suspect your board is bricked; I suggest updating the LPC Link2, but you may need a J-Link.

Recovering bricked LPC55Sxx EVK Boards | MCU on Eclipse

Best regards,
Pavel

0 Kudos
Reply

1,698 Views
VChaudhary
Contributor III

Hi,

I did mass erase using MCUXpresso IDE, but still, the board is not going in ISP mode.

Thanks

0 Kudos
Reply

1,744 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

I recommend trying to do a mass erase and then trying again to enter in ISP.

Best regards,
Pavel

0 Kudos
Reply

1,728 Views
VChaudhary
Contributor III

Hi,

Thanks for your reply,

I did mas erase using MCUXpresso IDE, but still, the board is not going in ISP mode.

 

Thanks

0 Kudos
Reply