LPC5536-EVB VER.C DEBUG ERROR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5536-EVB VER.C DEBUG ERROR

1,295件の閲覧回数
luna_liang
Contributor II

 

DEARS,

After build,when debug,it show DEBUG ERROR ,please help check,thank you.

 

 

luna_liang_0-1713252522391.png

 

0 件の賞賛
返信
3 返答(返信)

1,251件の閲覧回数
luna_liang
Contributor II
THANK YOU HANG ZHANG. ISP DOWNLOAD OK.
Another quesition:
When i download AN13577SW ,I3C SENSOR NETWORK
MY EVB is ver.C,then open R117,R123,TEST I3C wave, then no data and clock is 50M hz WAVE,so please help suggest how to test I3C singles,thank you.
0 件の賞賛
返信

1,241件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi
You can refer to LPCXpresso5536_EVK-DESIGN-FILES.
(1) SDA SIGNAL

HangZhang_0-1713426666175.png

You can measure JP77(1) or JP77(2).

(2) SCL SIGNAL

HangZhang_1-1713426774288.png

You can measure JP7(1).

Hope this will help you.

BR

Hang

 

 

0 件の賞賛
返信

1,264件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @luna_liang 

I can reproduce this error message, and the reason for this error is that you directly clicked on Start debugging project.
The I3C's pin is reused with SWD, which makes it impossible to debug SWD when using I3C.
So please use ISP mode to download image.
For specific operating steps, please refer to read me.

Hope this will help you.

BR

Hang

0 件の賞賛
返信