LPC5536-EVB VER.C DEBUG ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5536-EVB VER.C DEBUG ERROR

1,313 Views
luna_liang
Contributor II

 

DEARS,

After build,when debug,it show DEBUG ERROR ,please help check,thank you.

 

 

luna_liang_0-1713252522391.png

 

0 Kudos
Reply
3 Replies

1,269 Views
luna_liang
Contributor II
THANK YOU HANG ZHANG. ISP DOWNLOAD OK.
Another quesition:
When i download AN13577SW ,I3C SENSOR NETWORK
MY EVB is ver.C,then open R117,R123,TEST I3C wave, then no data and clock is 50M hz WAVE,so please help suggest how to test I3C singles,thank you.
0 Kudos
Reply

1,259 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi
You can refer to LPCXpresso5536_EVK-DESIGN-FILES.
(1) SDA SIGNAL

HangZhang_0-1713426666175.png

You can measure JP77(1) or JP77(2).

(2) SCL SIGNAL

HangZhang_1-1713426774288.png

You can measure JP7(1).

Hope this will help you.

BR

Hang

 

 

0 Kudos
Reply

1,282 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @luna_liang 

I can reproduce this error message, and the reason for this error is that you directly clicked on Start debugging project.
The I3C's pin is reused with SWD, which makes it impossible to debug SWD when using I3C.
So please use ISP mode to download image.
For specific operating steps, please refer to read me.

Hope this will help you.

BR

Hang

0 Kudos
Reply