LPC552x/S2x: The number of DMA transfers per request or trigger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC552x/S2x: The number of DMA transfers per request or trigger

559 Views
dmaeda
Contributor I

I would like to test burst transfer based on the DMA channel chain transfer example in the SDK, but the example seems to behave like burst transfer with single transfer (default).

I understand the number of transfers per request or trigger as follows:

If software trigger is used (SWTRIG=1), transfers are performed until descriptors are exhausted (RELOAD=0) or trigger is cleared (CLRTRIG=1).

If DMA request is used (PERIPHREQEN=1), a transfer is performed per request.

If hardware trigger is used with edge trigger (HWTRIGEN=1, TRIGTYPE=0), a transfer is performed per trigger with single transfer (TRIGBURST=0) or the number of transfers defined by BURSTPOWER is performed per trigger with burst transfer (TRIGBURST=1).

Is my understanding correct?

The DMA channel chain transfer example in the SDK seems that transfers continue until the descriptor is exhausted with the single transfer.

Best regards,

Daisuke

 

0 Kudos
6 Replies

530 Views
dmaeda
Contributor I

I have contacted TIC support about this.

0 Kudos

541 Views
dmaeda
Contributor I

Hi,

I modified the DMA channel chain transfer example for HW trigger and tested it, it seems that transfers by per trigger with single transfer (TRIGBURST=0) are performed until descriptors are exhausted (RELOAD=0) or trigger is cleared (CLRTRIG=1).

Why do the single transfer show this behavior in the example?

The modified example source code is attached.

HW trigger connection in the modified example:
PINT (P1_9 to low by S3 on LPC55S28-EVK) -> DMA0CH0 -> DMA0CH1 -> DMA0CH2

On the other hand, it worked as expected with burst transfer (TRIGBURST=1).

Best regards,

Daisuke

 

0 Kudos

507 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, let me review your case and when I have more information, I will contact you.

Best regards,
Pavel

0 Kudos

494 Views
dmaeda
Contributor I

Dear Pavel-san,

Thank you for your reply and daily support.

I would appreciate it if you respond to my case in TIC instead of this case.

Best regards,

Daisuke

 

0 Kudos

473 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I saw you have 3 cases with some differences in the DMA, for quality of service I will be following your case in one of these.

Best regards,
Pavel

0 Kudos

468 Views
dmaeda
Contributor I
Dear Pavel-san,

Thank you for your reply and daily support.

I would appreciate it if you respond to my cases in TIC.

Could you close this case?

Best regards,

Daisuke
0 Kudos