LPC5528 JTAG circuit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC5528 JTAG circuit

跳至解决方案
2,699 次查看
yuto
Contributor I

Hi.

Can you tell me about JTAG on the LPC5528?
Is writing programs in JTAG supported?
If so, please tell me about the schematic connections.

Preferred usage
Program writing in JTAG
Debugging with SWD
Write the program at SPI during ISP Boot

image.png

标签 (1)
0 项奖励
回复
1 解答
2,668 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

We use SWD and debug and program.

ISP boot code is in boot ROM, user can't reprogram boot ROM

在原帖中查看解决方案

4 回复数
2,687 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi yuto

Here is a very classic article for JTAG/SWD design

https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565#M44

 

Note that, for LPC5528, JTAG is used on this device for boundary scan and production test ONLY and
cannot to used for debugging purposes.

 

Have a nice day,

Jun Zhang

0 项奖励
回复
2,679 次查看
yuto
Contributor I

Thank you, Jun Zhang, for your reply!

Tell me more.

>"JTAG is used on this device for boundary scan and production test ONLY"

Flash Programming in JTAG is not possible?

How to programming the firmware you have created is ISP boot?
(UART,SPI,USB,etc..)

0 项奖励
回复
2,669 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

We use SWD and debug and program.

ISP boot code is in boot ROM, user can't reprogram boot ROM

2,661 次查看
yuto
Contributor I

Thank you, Jun Zhang, for your reply!

I understand.

0 项奖励
回复