Hi,
Regarding your question about the FC10 high speed SPI module, I recommend you use LPC54628-EVK board and have a try.
This is the FC10 high speed SPI module pin assignment:
PIO1_3 FC10_SCK
PIO1_1 FC10_MOSI
PIO1_2 FC10_MISO
PIO0_26 FC10_SSEL0
PIO2_22 FC10_SSEL1
PIO2_23 FC10_SSEL2
PIO2_24 FC10_SSEL3
On the EVK board, the PIO2_22,PIO2_23,PIO2_24 pins are connected to LCD, but are NOT connected to a connector.
On the LPC54628-EVK board, because the application code is saved/run in on-chip Flash, the on board SPIFI flash is not required to use, so you can configure the PIO0_26 as FC10_SSEL0 function.
pin assignment of FC10 for LPC54628-EVK board
PIO1_3 FC10_SCK, pin 16 of J13 with pin2&3 closed for JS26
PIO1_1 FC10_MOSI pin12 of J12
PIO1_2 FC10_MISO pin 18 of J13 with pin 2&3 closed for JS25
PIO0_26 FC10_SSEL0 pin2 of J13

Hope it can help you
BR
XiangJun Rong