We have plan to make our new product using LPC546xx.
We want to use external parallel NAND flash to store a lot of sensor data about 128 MB - 1 GB.
According to below discussion, EMC supported LPC can support external parallel NAND flash.
https://community.nxp.com/message/762682
Can LPC546xx also support external parallel NAND flash?
Please reply as soon as possible.
Best regards,
Takashima
According to the following discussion, LPC4367 can support external parallel NAND flash.
NAND Flash interface support in LPC4367
Why EMC of LPC546xx cannot support external parallel NAND flash?
Please reply as soon as possible.
Best regards,
Takashima
 
					
				
		
 xiangjun_rong
		
			xiangjun_rong
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi, Isao,
I do not think that the EMC of LPC54xxx supports nand flash, the EMC supports only SDRAM,SRAM,parallel Nor flash,I suggest you use i.mxrt family for example i.mxrt1020/1050, which has SEMC module,can interface with NOR flash, SRAM,SDRAM,Nand flash.
i.MX RT Series: MCU/Applications Crossover Processor | Arm® Cortex®-M7 | NXP
Hope it can help you
BR
XiangJun Rong