LPC546xx DMA Channel Chain CH x exhausted and trigger CH y

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC546xx DMA Channel Chain CH x exhausted and trigger CH y

1,280 Views
A_M
Contributor III

Hello,

I need to trigger DMA channel y when channel x is exhausted.

I use the example project lpcxpresso54628_dma_channel_chain for a test and UM10912 Rev 2.4

 

The function should be:

Ch X start the transfer with a software trigger (later adc) and transfer a uint32_t (4Byte) value. After three triggers (12Byte) Ch x is exhausted, sets a trigger (for Ch y) and reload the ch x descriptor.

Ch y transfer uint32_t (4Byte) after two trigger from Ch x the Ch y is also exhausted and reload the ch y descriptor.

 

I not able implement this function.

My example project never triggers ch y when ch x is exhausted.

Or when I comment in Line 90 INPUTMUX->DMA_OTRIG_INMUX[0] = 0; //ch0 is always triggers ch y when I trigger ch x.

I don’t get it what do I have to set let it word properly.

 

How do I have to set the DMA?

Tags (2)
0 Kudos
Reply
6 Replies

812 Views
A_M
Contributor III

Hello @Alice_Yang , I wanted to ask how far the status is?

BR

A_M

0 Kudos
Reply

1,108 Views
A_M
Contributor III

Hello @Alice_Yang ,

are there any novelties for me?

BR

A_M

0 Kudos
Reply

1,228 Views
A_M
Contributor III

Hello @Alice_Yang 

I made a project with less changes and committed the changes.

CH0 is configurated as BurstSize1(before kDMA_SingleTransfer).

Line 163 Trigger CH0. It should not start/trigger other channels. When it Triggered once.

I found a post here. Like I understand, matt83 wanted to use the DMA in the same way as I do. I guess the DAM works on both MCUs in the same way. What was the solution for his Problem?

https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S16-DMA-done-trigger-event/td-p/1785082

0 Kudos
Reply

1,253 Views
A_M
Contributor III

Hello @Alice_Yang ,

yes it works fine.

My SDK Version is 2.16 Mainfest Version 3.14.0

BR

Alex

 

0 Kudos
Reply

1,231 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @A_M 

Your project is based on the SDK demo, I will test it on my setup. Could you also share the key modifications you’ve made to the original code? This will help me pinpoint issues more efficiently. Thank you!

 

BR

Alice

0 Kudos
Reply

1,265 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @A_M 

Has the SDK demo ​lpcxpresso54628_dma_channel_chain been functioning as expected in your environment?

 

BR

Alice

0 Kudos
Reply