LPC546XX ADC Peripheral Clock Frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC546XX ADC Peripheral Clock Frequency

跳至解决方案
1,253 次查看
guitardenver
Contributor IV

I have a question about the LPC546 MCU.

The datasheet says the max ADC clock frequency is 80MHz.

"In the synchronous operating mode, this ADC clock is derived from the system clock.
In this mode, a programmable divider is included to scale the system clock to the
maximum ADC clock rate of 80 MHz."

pastedImage_1.png

Question:
1) Can the input to the ADC CLOCK DIVIDER be 180MHz since my pll_clk is? Or does the 80MHz limit apply to both before and after that divider block?

标记 (3)
0 项奖励
回复
1 解答
1,150 次查看
soledad
NXP Employee
NXP Employee

Hi,

The ADC clock is based on the output of the ADC clock divider ADCCLKSEL in the SYSCON block. The maximum ADC clock frequency must not exceed 80 MHz.


Have a great day,
Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,151 次查看
soledad
NXP Employee
NXP Employee

Hi,

The ADC clock is based on the output of the ADC clock divider ADCCLKSEL in the SYSCON block. The maximum ADC clock frequency must not exceed 80 MHz.


Have a great day,
Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复