LPC54618: Hard Fault When entering DeepSleep

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC54618: Hard Fault When entering DeepSleep

跳至解决方案
2,279 次查看
AleemS
Contributor II

When trying to enter deepsleep mode on the LPC54618 an HardFault occurs. Going through step by step with gdb the instruction

0x200058e0 <+0>: push {r4, r5, r6, r7, lr}

in the function relocMem.8033 causes the HardFault. The Main stack starts at 0x200044a8 and has Size 0x1000. I have tried calling POWER_EnterDeepSleep with arguments uint64_t(-1), 0, and

(uint64_t(SYSCON_PDRUNCFG_PDEN_SYSOSC_MASK | SYSCON_PDRUNCFG_PDEN_EEPROM_MASK) << 32) |
        (SYSCON_PDRUNCFG_PDEN_SRAMX_MASK | SYSCON_PDRUNCFG_PDEN_SRAM0_MASK |
         SYSCON_PDRUNCFG_PDEN_SRAM1_2_3_MASK | SYSCON_PDRUNCFG_PDEN_VD6_MASK), which expands to 0x28'2000'E000.

Context:

++ MbedOS Fault Handler ++

FaultType: HardFault

Context:
R 0: FFFFFFFF
R 1: FFFFFFFF
R 2: 00000000
R 3: 200058E1
R 4: 20002BC4
R 5: 00000008
R 6: 20005474
R 7: 000084A1
R 8: 200030C4
R 9: 00000001
R 10: 00021744
R 11: 00000000
R 12: 200058E0
SP : 20005438
LR : 000088A5
PC : 200058E0
xPSR : 610F0000
PSP : 200053D0
MSP : 20027FC0
CPUID: 410FC241
HFSR : 40000000
MMFSR: 00000001
BFSR : 00000000
UFSR : 00000000
DFSR : 00000000
AFSR : 00000000
Mode : Thread
Priv : Privileged
Stack: PSP

-- MbedOS Fault Handler --

 

++ MbedOS Error Info ++
Error Status: 0x80FF013D Code: 317 Module: 255
Error Message: Fault exception
Location: 0x200058E0
Error Value: 0x20005538
Current Thread: main Id: 0x20004460 Entry: 0x111A1 StackSize: 0x1000 StackMem: 0x200044A8 SP: 0x20005438
For more info, visit: https://mbed.com/s/error?error=0x80FF013D
-- MbedOS Error Info --

标记 (1)
0 项奖励
回复
1 解答
2,144 次查看
AleemS
Contributor II

Hello,

i have solved the problem. In Order to call POWER_EnterDeepSleep in an mbed-os Program you have to create an mbed::ScopedRamExecutionLock inside the Scope that needs to execute from RAM. Otherwise the execution will cause a Hardfault because of the MemoryProtectionUnit. It might be similarly handled in other Real-Time-Operating-Systems.

This also seems to eliminate all Problems with the Interrupts.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,212 次查看
AleemS
Contributor II

Unfortunately it still HardFaults just at another address (due to the build being a different one) but the same instruction. Running the underlying function DeepSleepReloc directly does not cause a hard fault.

0 项奖励
回复
2,204 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As the following figure of LPC546xx memory map, the address 0x2000_xxxx are SRAM, for the error code:0x200058e0 <+0>: push {r4, r5, r6, r7, lr}, it appears that you allocate/execute the code in SRAM instead of Flash, while you allocate main stack in address 0x200044a8, as you see the code address(0x200058e0) and stack address(0x200044a8) are approaching, I guess that the code is overlapped with stack, that is why you get the hard-fault error, but it is only guess.

Pls try to allocate the application code in flash instead of SRAM or the other SRAM address and have a try.

BR

XiangJun Rong

xiangjun_rong_0-1689216085869.png

 

0 项奖励
回复
2,194 次查看
AleemS
Contributor II

Is it possible, that calling the function directly from flash, corrupts the system state and makes interrupts impossible?

Because after calling the function from Flash i cannot cause the chip to wake up from deepsleep.

0 项奖励
回复
2,150 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi

As you know that the LPC546xx uses interrupt mechanism to wake-up the processor from deep-sleep state, so you have to set up the ISR of the waking-up  source. I suggest you run all the code in flash.

Anyway, in SDK, NXP provides power_manager_lpc example, which is fully tested,  If you run the power_manager_lpc example directly, do you have any issue?

BR

XiangJun Rong

0 项奖励
回复
2,145 次查看
AleemS
Contributor II

Hello,

i have solved the problem. In Order to call POWER_EnterDeepSleep in an mbed-os Program you have to create an mbed::ScopedRamExecutionLock inside the Scope that needs to execute from RAM. Otherwise the execution will cause a Hardfault because of the MemoryProtectionUnit. It might be similarly handled in other Real-Time-Operating-Systems.

This also seems to eliminate all Problems with the Interrupts.

0 项奖励
回复
2,234 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you run the power_manager_lpc example directly, do you have any issue?

This is the code in above example when you enter deep sleep:

#define APP_EXCLUDE_FROM_DEEPSLEEP \
(SYSCON_PDRUNCFG_PDEN_SRAMX_MASK | SYSCON_PDRUNCFG_PDEN_SRAM0_MASK | SYSCON_PDRUNCFG_PDEN_SRAM1_2_3_MASK)

case kPmu_Deep_Sleep: /* Enter deep sleep mode. */

POWER_EnterDeepSleep(APP_EXCLUDE_FROM_DEEPSLEEP);

break;

Pls have a try

BR

XiangJun Rong

0 项奖励
回复