LPC54608 Secondary bootloader jump and main app debugging

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54608 Secondary bootloader jump and main app debugging

3,043 次查看
cybaluke
Contributor III

Hi, i'm working with LPC54608 and MCUxpresso, I have already coded my main application and now I have to code a secondary bootloader, so I have some question about this:

1 - first I've moved the main app at the 0x8000 address (32kB sector) in flash using the MCUxpresso's memory setting option, but now I can't debug this app because when I launch the debug session the debugger doesn't break in the main function but jumps in a wrong RAM location (the flash memory from 0x0 to 0x7FFF is empty). What I'm missing to correctly debug the main relocated app?

2 - For my Secondary Bootloader first step I've tryed to make a bootloader that only should jump immediatly at the main app (at the flash address 0x8000) but I have some problems with the jump so  what is the right calling code to jump from  the secondary bootloader to main app?

3 - what is the right code to jump back from main app to the bootloader at 0x00000000 address?

4 - is it possible automatically upload the SecondaryBootloader firmware together the main app during the main app debugg session  launch?

标签 (3)
3 回复数

2,155 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Cybaluke,

Which debugger connection are you using?  

I would recommend you to use the LPC1700 secondary USB bootloader as reference:

http://cache.nxp.com/docs/en/application-note/AN10866.zip

This is the function used by the bootloader to jump to the application:

__asm void boot_jump( uint32_t address ){
   LDR SP, [R0]        ;Load new stack pointer address
   LDR PC, [R0, #4]    ;Load new program counter address
}

 

You can debug both the bootloader and the application by adding the following command to your debug Run Commands in the bootloader debug connection:
add-symbol-file filename address
As an example:

 

add-symbol-file C:\\Users\\Documents\\MCUXpressoIDE_10.xxx\\workspace\\MK64FN1M0xxx12_Project_2\\Debug\\MK64FN1M0xxx12_Project_2.axf 0x80000

 

pastedImage_1.png

 

The address 0x80000 corresponds to the first flash section of the second project which was previously flashed to the MCU:

 

pastedImage_3.png


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复

2,155 次查看
cybaluke
Contributor III

Any comment about my reply/question?

thanks Carlos for the answer,

but.... I'm using the MCUXpresso LinkServer Debugger with the OM13092 lpclink onboard debugger for my first tests and then I use an LPC_LINK2 debugger for my custom target board (via SWD connection), so I can't find the "add-symbol-file filename address" equivalent settings you suggested for my debug configurations. I think your solution is right for the Segger debug interface, isn't it?

Is there an equivalent solution for the LinkServer debugger configuration for loading and debugging both the bootloader (@0x0000 address) and the main app (@0x8000 address) projects?

0 项奖励
回复

2,155 次查看
cybaluke
Contributor III

thanks Carlos for the answer,

but.... I'm using the MCUXpresso LinkServer Debugger with the OM13092 lpclink onboard debugger for my first tests and then I use an LPC_LINK2 debugger for my custom target board (via SWD connection), so I can't find the "add-symbol-file filename address" equivalent settings you suggested for my debug configurations. I think your solution is right for the Segger debug interface, isn't it?

Is there an equivalent solution for the LinkServer debugger configuration for loading and debugging both the bootloader (@0x0000 address) and the main app (@0x8000 address) projects?