LPC54608 RS485 example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54608 RS485 example

2,726 次查看
rolandhösch
Contributor I

Is there any example out there who to configure a flexcomm USART port of the LPC54608 for serial RS485 communication?

标签 (1)
标记 (1)
2 回复数

1,709 次查看
primate
Contributor III

Opening the thread again since I am planning to get the LPCXpresso54628 Development Board but I am not sure how to implement the RS485 protocol entierly.

Also, I found an example RS485 and I presume the code can be modified to fit into the LPCXpresso54628 

Two LPC1765 devices communicating through RS-485? 

Thank for any help.

0 项奖励
回复

1,709 次查看
soledad
NXP Employee
NXP Employee

Hi,

We only have the SDK for LPC54608 examples.


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复