LPC54608 M1pin(port1,20) cannot ON-OFF

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54608 M1pin(port1,20) cannot ON-OFF

656件の閲覧回数
実奥山
Contributor II

 tried onoff test of IO port. It is M1-pin,(port1,20).

Other pins do on-off.

But M1 pin do not   on-off.

Below is a sample program.

port(1,17)  do on-off.

But port(1,20 M1 pin) do not   on-off.

    GPIO_Clken(1);         /* GPIO1 CLK enable */

GPIO_PinInit(1,17, &output_config);  

GPIO_PinInit(1,20, &output_config);

 

               oPort_sub(1,17,1);
               oPort_sub(1,17,0);

               oPort_sub(1,20,1);
               oPort_sub(1,20,0);

Please teach me how to control  M1-pin,(port1,20).

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

560件の閲覧回数
実奥山
Contributor II

jeremyzhou-san

Thank you.

Only PIO1_17 can output the low(0V) or high(3.3V)level,

But PIO1_20 output only hjgh(3.3V).

Later  I confirmed that PIO1_21 output only hjgh(3.3V) too.

I cannot control PIO1_20 and PIO1_21. 

okuyama

0 件の賞賛
返信

560件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi 実 奥山,

Thanks for your reply.
It seems a bit weird.
Whether you can upload the complete sample code, meanwhile, I'd highly recommend you to refer to the gpio demo in the SDK library.
You can download the SDK library via the below link.
https://mcuxpresso.nxp.com/en/welcome

Have a great day.

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

560件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi 実 奥山,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
According to the description, you want to configure the PIO1_17 and PIO1_20 as the GPIO, however, only PIO1_17 can output the low or high level, is it right?

pastedImage_2.png
Whether you can upload the complete sample code, meanwhile, I'd highly recommend you to refer to the gpio demo in the SDK library.
You can download the SDK library via the below link.
https://mcuxpresso.nxp.com/en/welcome

Have a great day.

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信