LPC54608 Hard Fault (The value of on-chip-flash has been changed)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54608 Hard Fault (The value of on-chip-flash has been changed)

2,794件の閲覧回数
mega32
Contributor II

Hello everybody, today I discovered a puzzling Hard Fault problem on the NXP LPC54608 MCU.

 

At present, during our testing process, we have found that out of 18000 MCU machines, 500 MCU machines have experienced hard faults.

Surprisingly, each MCU machine has a different PC address where the error occurred, but the same MCU machine that has experienced hard faults will repeatedly experience hard faults at the same PC address.

In fact, the current MCU machine with hard fault is one of 500 MCU machines that have experienced hard fault. The following is a description of the problem with this MCU machine.

 

"0xf8df0a48"(correct code) is the content on program code segment 0x00004120 (on-chip-FLASH's address).

IAR memory_correctIAR memory_correct

When I debug and execute code (running code on on-chip-flash), everything seems to be running smoothly from the beginning.

However, at the moment Function A returns, the content of program code segment 0x00004120 has been changed from "0xf8df0a48" to "0xf8df0848". (I don't know why this is happening, I would like to ask for your opinion)

IAR disassemblyIAR disassemblyFunction AFunction AIAR memory_errorIAR memory_error

Therefore, a hard fault interrupt occurred while executing code "0xf8df0848" (which should have executed “0xf8df0a48"), and after entering the hard fault interrupt, the content of program code segment 0x00004120 changed from the wrong "0xf8df0848" to the correct "0xf8df0a48" again, which felt too incredible!

6 返答(返信)

2,092件の閲覧回数
Km10
Contributor I

Hello @mega32 

It seems that we're experiencing exactly the same issue with our products equipped with the same MCU. We have very similar defect rates.

Have you found a solution to this issue? Have you implemented any safeguards to prevent falling into this situation again?

Thank you in advance for your help and have a good day!

0 件の賞賛
返信

2,747件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @mega32 

How about tested with simple demo code? Or other projects?

Also change to other IDE to test, for example MCUXpresso IDE.

 

BR

Alice

0 件の賞賛
返信

2,711件の閲覧回数
mega32
Contributor II

Hi @Alice_Yang

Thank you for your answer,

I tried using simple demo code, but I can't reproduce this problem.

I am using IAR's non download debugging to reproduce this problem, and I think it should not be related to the IDE.

BR

Mega32

0 件の賞賛
返信

2,661件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @mega32 

If only the specified project and IDE can reproduce issue, recommend you check code and optimization level.

 

BR

Alice

0 件の賞賛
返信

2,643件の閲覧回数
mega32
Contributor II

Hello @Alice_Yang

We have checked the code many times and there are no issues.
Meanwhile, the optimization level is set to 'None'.

Moreover, this Hard Fault problem is only an occasional occurrence (500/18000), and it should not be caused by the reason you mentioned.

BR
mega32

0 件の賞賛
返信

2,506件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @mega32 

If only some of them have issue, recommend you contact your distributor.

 

BR

Alice

0 件の賞賛
返信