LPC54606 in QFP100 package and SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54606 in QFP100 package and SDRAM

Jump to solution
2,322 Views
carstengroen
Senior Contributor II

The LPC54606 comes (also) in a QFP100 package. It is shown in the datasheet that it supports 8/16 bit EMC interface. It has support for port 0 and port 1 so most of the EMC (for SDRAM) signals are there.

However, the EMC_A[14] are only located on P3.25 which is not available on the 100 pin package. EMC_A[13] and EMC_A[14] are connected to BA0 and BA1 on a 16 bit SDRAM device. Is there some different connections to be used on the 100 pin package, or is it not possible to support 16 bit SDRAM on this package ?

Labels (2)
0 Kudos
Reply
1 Solution
1,884 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Carsten Groen,

The EMC supports 8/16 bit data bus on BGA100 package, you can learn the more information about the SDRAM interface to LPC546xx external memory controller via the application note.

http://www.nxp.com/docs/en/nxp/application-notes/AN12026.pdf 

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,884 Views
carstengroen
Senior Contributor II

Could really use a hint regarding this....

0 Kudos
Reply
1,885 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Carsten Groen,

The EMC supports 8/16 bit data bus on BGA100 package, you can learn the more information about the SDRAM interface to LPC546xx external memory controller via the application note.

http://www.nxp.com/docs/en/nxp/application-notes/AN12026.pdf 

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,884 Views
carstengroen
Senior Contributor II

Thanks a lot Jeremy!

I was not aware of that application note (I see it went online 2 days before my original question :smileywink:), the text:

pastedImage_1.png

explains it perfectly, thanks :smileyhappy:

0 Kudos
Reply