LPC546 MCAN not sending data continuously.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC546 MCAN not sending data continuously.

1,478 Views
emb02
Contributor V

I am trying to interface MCAN and want to send data continuously but when I disconnect CAN H or CAN L line it will sets error and giving kStatus_MCAN_TxBusy status. it is not giving idle status when i connect line again. please help me to continuous communication between CAN. I am initiating can using config tools.

Labels (2)
Tags (3)
0 Kudos
Reply
3 Replies

1,460 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

What do you mean "when I disconnect CAN H or CAN L line"? do you means that you disconnect both the CAN H or CAN L line between transmitter and receiver nodes?

BR

XiangJun Rong

0 Kudos
Reply

1,455 Views
emb02
Contributor V
yes I am disconnecting CAN H, CAN L .
0 Kudos
Reply

1,451 Views
frank_m
Senior Contributor III

Educate yourself about the meaning of transmit / receive errors, error passive state, and bus-off state, which are intrinsic part of the CAN specification.

0 Kudos
Reply