LPC54102 power rail leakage?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54102 power rail leakage?

1,082 Views
StephenYeh
Contributor III

Hi,

Is it possible that power rail design

@ VDDA:3.3V / VDD:1.8V / VREFN: 0V / VREFP:2.5V ?

We got the issue that VDD will leakage to 2.3V.

 

StephenYeh_0-1660053260817.png

 

 

0 Kudos
Reply
3 Replies

1,079 Views
StephenYeh
Contributor III

Hi,

I check the spec.(the leakage will from VIA design(it will refer. VDD) right?

StephenYeh_0-1660092919193.png

 

 

0 Kudos
Reply

1,038 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi StephenYeh 

This issue is linked with a internal ticket. I will keep you informed if any update.

For now, I suggest you setting VDDA equal to VDD.

Thanks,

Jun Zhang

0 Kudos
Reply

983 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @StephenYeh 

In the limiting table, the analog input voltage should say VDDA instead of VDD. When the ADC is used, the signal levels signal levels on analog input pins must not be above the level of VDDA at any time.

Hope this helps,

Jun Zhang

0 Kudos
Reply