LPC5410 IO rising time too small

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC5410 IO rising time too small

1,056 次查看
Twang
Contributor I

     Hello, I am a hardware engineer. When using your company's LPC5410 chip, I have some questions about the parameters of I/O pins in the datasheet.
    The tr and tf of the pin configured as input as described in 11.3 of the specification are between 0.3ns-1.3ns and 0.2ns-1.2ns. The data performance in the test process or tr and tf of the chip's own IO output are relatively small. May I ask if there is any error or update in the datasheet?

标记 (2)
0 项奖励
回复
2 回复数

1,021 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Of course, the data sheet can specifies the rising time and falling time of only output pins with predefined load capacitor, it can not specify the rising time and falling time of input pins, because the  rising time and falling time of input pin is only dependent on the external  source driving capability and the load capacitor.

So this is a typo of the documentation.

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复

1,051 次查看
Twang
Contributor I
 
0 项奖励
回复