LPC54018, JLink, IAR I cannot flash hello_world

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54018, JLink, IAR I cannot flash hello_world

850 Views
danielgull
Contributor IV

Hi

I am having trouble to flash hello world onto my target board LPC54018 OM40003.

I am trying to flash the demo application

SDK_2.7.0_LPCXpresso54018\boards\lpcxpresso54018\demo_apps\hello_world\iar\hello_world.eww

using the following toolchain: IAR 8.22.1.15700 and CMSIS DAP with the onboard Debug Link and a USB cable connected to the PC. However I cannot flash at all. I get a pop up window with the CMSIS-DAP error message "Fatal error: Probe not found. How can I get this board up and running so that I can work with it? This is already the second board that is not working out of the box.

Many thanks

Dani

0 Kudos
2 Replies

743 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Daniel Gull,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Regarding your issue, I'd like to suggest you try the following steps to fix the issue.
1. Please assure the hardware setup is correct via referring to the attachment.
2. Update the firmware of the on-board Debug Probe.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

743 Views
danielgull
Contributor IV

Hi Jeremey,

I updated according to the attached manual and the system is running again. I will continue to moitor the situation.

Many thanks

Dani

0 Kudos